6/18/2018 11:47 AM | |
Posts: 8 Rating: (0) |
I have copied the code to an txt file so indents remain. See attachment Anyone has an idea how to copy SCL code to this forum so indentation remains ? Kind regards Cedric AttachmentSCL_CODE_1.txt (143 Downloads) |
6/18/2018 11:29 PM | |
Joined: 7/7/2010 Last visit: 4/25/2024 Posts: 14628 Rating: (2348)
|
If you name the file as .scl.txt, we know automatically the file contains SCL. Attached is your SCL, successfully compiled in V15 on a S7-1500 PLC without all the messiness of external items. This block is your block as I would write it during the first or second draft. Save this "as" a .scl file to a common folder, like "your documents / automation / forums / comm_test_fb.scl" You can import it directly into your project and look at it. To do that, with your project open, expand the project tree so you can see the > left of "External source files". Click the arrow to expand that selection. Click Add new external file, follow prompts and import that scl file. This is the contents in case you are curious (or nervous):
With an attachment the original indentation remains. Other than that, I should probably know a better answer, but slamming the space bar a lot seems to do the trick for me. I hope someone else can shame me with the right answer.
AttachmentComm_Test_SCL_FB.scl.txt (89 Downloads) |
science guy |
|
Follow us on