4/28/2016 5:12 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
Hello Jackcaress, which RT do you use? Still Comfort panel of some size? Do the "3" screens have the same I/Os and only the values differ or are they completely different? You can use a faceplate (https://support.industry.siemens.com/cs/ww/en/view/68014632) and make the visibility depending on a tag that is set according to the shape: Shape A : VisibilityTag = 1 In the faceplate: Use the layers wisely and make the visibility of the objects dependent on the VisibilityTag value. If you put each instance of the faceplate onto a popup screen you don't have to create a new screen for every instance and you can call them in the same screen. |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
4/28/2016 5:15 PM | |
Joined: 3/12/2015 Last visit: 11/29/2023 Posts: 529 Rating: (15) |
|
4/28/2016 5:53 PM | |
Joined: 3/12/2015 Last visit: 11/29/2023 Posts: 529 Rating: (15) |
Looking over what you said H.J it was possible just to replace some of the data with simple visibility varibles thank you |
4/29/2016 9:54 AM | |
Joined: 3/12/2015 Last visit: 11/29/2023 Posts: 529 Rating: (15) |
Thats what i ended up doing, instead of creating loads of unnessary pages i just changed the image, cheers |
Follow us on