Industry Online Support
Technical Forum
5/9/2007 11:43 AM | |
Posts: 83 Rating: (8) |
Hallo All, I am using WinCC v6.0 SP4 HF3 OS is XP SP2 When I start WinCC in runtime I got error message like attachment. In SCRIPT.LOG I found this: //==================================================================== // WinCC reported exception with code: C0000005 ACCESS_VIOLATION // Date: 8.5.2007 - Time: 22.38.54 // Caused at logical address 7C910F29 01:0000FF29 //==================================================================== // FAULTING MODULE: C:\WINNT\system32\ntdll.dll //==================================================================== // Registers: // ---------- // EAX:02278E50 // EBX:003B0000 // ECX:00000040 // EDX:00000011 // ESI:02278E48 // EDI:02276FC8 // CS:EIP:001B:7C910F29 // SS:ESP:0023:010DF2B4 EBP:010DF2C0 // DS:0023 ES:0023 FS:003B GS:0000 // Flags:00010246 // // Call stack: // ----------- // Address | Frame | // ---------+----------+---------------------------------------------- // 7C910F29 | 010DF2C0 | wcsncpy+49A // 7C918251 | 010DF2F8 | RtlReAllocateHeap+854 // 7C911C76 | 010DF528 | RtlInitializeCriticalSection+149 // 77C2C3C9 | 010DF568 | free+1AE // 77C2C3E7 | 010DF574 | free+1CC // 77C29CD4 | 010DF584 | operator new+F // 72FA1FEF | 010DF5A4 | 0001:00000FEF C:\Program Files\Siemens\WinCC\bin\OHIOIPC.dll // 72FA1735 | 010DF5EC | 0001:00000735 C:\Program Files\Siemens\WinCC\bin\OHIOIPC.dll // 77D48734 | 010DF618 | GetDC+6D // 77D48816 | 010DF680 | GetDC+14F // 77D4B4C0 | 010DF6D4 | DefWindowProcW+184 // 77D5E7FE | 010DF704 | GetGUIThreadInfo+55 // 7C90EAE3 | 010DFF44 | KiUserCallbackDispatcher+13 // 72FA11FD | 010DFF80 | 0001:000001FD C:\Program Files\Siemens\WinCC\bin\OHIOIPC.dll // 77C3A3B0 | 010DFFB4 | endthreadex+A9 // 7C80B683 | 010DFFEC | GetModuleFileNameA+1B4 //==================================================================== //==================================================================== // WinCC reported exception with code: C0000005 ACCESS_VIOLATION // Date: 9.5.2007 - Time: 10.55. 9 // Caused at logical address 7C91888F 01:0001788F //==================================================================== // FAULTING MODULE: C:\WINNT\system32\ntdll.dll //==================================================================== // Registers: // ---------- // EAX:0283E000 // EBX:027E0000 // ECX:02BE0000 // EDX:00006569 // ESI:02BE0110 // EDI:0286F0E8 // CS:EIP:001B:7C91888F // SS:ESP:0023:010DF4C4 EBP:010DF4D8 // DS:0023 ES:0023 FS:003B GS:0000 // Flags:00010287 // // Call stack: // ----------- // Address | Frame | // ---------+----------+---------------------------------------------- // 7C91888F | 010DF4D8 | RtlReAllocateHeap+E92 // 7C918238 | 010DF510 | RtlReAllocateHeap+83B // 7C911C76 | 010DF740 | RtlInitializeCriticalSection+149 // 77C2C3C9 | 010DF780 | free+1AE // 77C2C3E7 | 010DF78C | free+1CC // 77C29CD4 | 010DF79C | operator new+F // 72FA1FEF | 010DF7BC | 0001:00000FEF C:\Program Files\Siemens\WinCC\bin\OHIOIPC.dll // 72FA1735 | 010DF804 | 0001:00000735 C:\Program Files\Siemens\WinCC\bin\OHIOIPC.dll // 77D48734 | 010DF830 | GetDC+6D // 77D48816 | 010DF898 | GetDC+14F // 77D4B4C0 | 010DF8EC | DefWindowProcW+184 // 77D5E7FE | 010DF91C | GetGUIThreadInfo+55 // 7C90EAE3 | 010DFF44 | KiUserCallbackDispatcher+13 // 72FA11FD | 010DFF80 | 0001:000001FD C:\Program Files\Siemens\WinCC\bin\OHIOIPC.dll // 77C3A3B0 | 010DFFB4 | endthreadex+A9 // 7C80B683 | 010DFFEC | GetModuleFileNameA+1B4 //==================================================================== Can anybody tell me whats wrong? I am a bit confuse here Thanks. AttachmentDrive_D.zip (106 Downloads) |
5/9/2007 1:24 PM | |
Posts: 3149 Rating: (171)
|
Hi please attach ALL files from folder ..\wincc\diagnose. nemo |
5/9/2007 1:29 PM | |
Posts: 83 Rating: (8) |
Hi Nemo, here are all logs. Thanks. AttachmentDiagnose.zip (115 Downloads) |
5/9/2007 1:49 PM | |
Posts: 3149 Rating: (171)
|
Hi there are some entries like this: 255,09.05.2007,09:55:14:932,1007000,4,,E51A1XHD,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,09.05.2007,09:55:24:933,1007000,4,,E51A1XHD,SCRIPT,ActionOverflow:more than 5000 Actions to work 255,09.05.2007,09:55:30:934,1007000,4,,E51A1XHD,SCRIPT,ActionOverflow:more than 5000 Actions to work => http://support.automation.siemens.com/WW/view/en/11965771 http://support.automation.siemens.com/WW/view/en/2357302 65535,09.05.2007,11:36:55:444,1001003,8,,E51A1XHD,PDLRuntimeSystem,,,0,0,0,Picture not found (MAT1500.PDL),,, 65535,08.05.2007,22:40:36:890,1001001,8,,E51A1XHD,PDLRuntimeSystem,,,0,0,0,Operator action not active (Navigation_MainGroup.Button6),,, 65535,08.05.2007,22:40:37:484,1001001,8,,E51A1XHD,PDLRuntimeSystem,,,0,0,0,Operator action not active (Navigation_MainGroup.Button7),,, 255,08.05.2007,14:17:27:868,1007001,4,,E51A1XHD,SCRIPT,ExecuteError in Action @91f 255,08.05.2007,14:17:28:009,1007001,4,,E51A1XHD,SCRIPT,ExecuteError in Action @8ac 255,08.05.2007,14:17:28:118,1007001,4,,E51A1XHD,SCRIPT,ExecuteError in Action @9a4 => http://support.automation.siemens.com/WW/view/en/8385493 2007-05-08 22:25:41,359 ERROR Connectionerror 1 "EAF": Errorcode 0x0000 7004! 2007-05-08 22:30:18,015 ERROR Connectionerror 2 "EAF": Errorcode 0x0000 7004! 2007-05-08 22:37:22,500 ERROR Connectionerror 3 "EAF": Errorcode 0x0000 7004! 2007-05-08 22:41:15,406 ERROR Connectionerror 4 "EAF": Errorcode 0x0000 7001! 2007-05-08 22:41:20,234 ERROR Cannot connect to "EAF": Errorcode 0x0000 7000! => http://support.automation.siemens.com/WW/view/en/22556102 A lot of work seems to wait for you..... nemo |
5/9/2007 2:41 PM | |
Posts: 83 Rating: (8) |
geee Nemo... thanks for explanation. 5000 actions are waiting for me |
Follow us on