6/2/2016 2:06 PM | |
Joined: 6/16/2015 Last visit: 2/22/2023 Posts: 29 Rating: (0) |
I decide a similar problem: I have connected to the SIMOREG via USB/COM USS connection and manage via PC. The DriveMonitor has a drive start\stop button and speed reference, but it is necessary HMI for the operator . To do this, there are scripts (two buttons). There are capter in User manual DriveMonitor "Integration
of VBScript into DriveMonitor" and there are some scripts. I try to test some of them, but i don't understand how to use FORM, WND, Integrate your own ActiveX controls, so don't create HMI for Operatore. If anybody have a script (HMI for operatore), please share. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/2/2016 5:07:59 PMNew subject after splitting the collective mind will prevail over common sense |
|
Follow us on