2/14/2015 3:21 PM | |
Joined: 12/13/2005 Last visit: 2/21/2025 Posts: 64 Rating:
|
Hello, I'm using a MP377 19" panel (A) (Wincc Flexible 2008) with a smartaccess license. Most of the time another MP377 19" (B) is connected as client. But sometimes another PC on the network makes an connection to (A). When later on panel (B) want to make a connection it gots the message that no more connections are possible. So first the PC needs to shutdown the connection. My question: is it possible that a script (that is triggered by a PLC-tag) can close al open smartclient connections? thanks already for your efforts. |
2/16/2015 3:34 PM | |
Joined: 8/3/2009 Last visit: 3/14/2025 Posts: 14990 Rating:
|
Hello Mr. Q-Bridge The only way to solve your problem is to restart the smart Server on the Server Panel. In this case the connections will be all disconnected. --> i Think this is the best way for you: 1.)create a Trigger Tag 2.)configure it to cyclic update 3.)use the trigger Value Change of this tag 4.)Use the systemfunction "ControlSmartServer" with parameter STOP 5.)Use another TriggerTag in the same way and START the Smart Server after a few seconds or a minute again. Then all connections are free again I hope it helps you. Have a nice day Bye Murof ------------ If this Information helps, you could use the Rate button |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
2/16/2015 4:12 PM | |
Joined: 12/13/2005 Last visit: 2/21/2025 Posts: 64 Rating:
|
Thanks for your solution. In my case where the 19" panel only support 1 client it is no problem to disconnect all connections. I'll thy it out at the end of this week. |
Follow us on