6/20/2008 5:50 PM | |
Posts: 2661 Rating: (279) |
Can you post your HW config (after exporting)? Thanks. |
12/3/2008 11:16 AM | |
Posts: 1 Rating: (0) |
While Commissioning of cement plantwith CPU 416-3DP using CP443-5 Order No 6GK7 443-5DX04-0XE0 during the hardware configuration of Simocode ProVin the profibus when the number of Simocode Pro Vexceedesmore than 74 nodes SDB error arrives "The size of section 1 of SDB 126 exceeds 64 KB" I have attached HW Configuration Export File Anypossible solution to overcome the issue. Regards, Subramani Attachmentplc#3.zip (92 Downloads) |
12/4/2008 2:25 AM | |
Posts: 2661 Rating: (279) |
See if this helps: How do you clear the message "Maximum length of code area reached (max. 64 Kbytes)"? |
Follow us on