4/18/2012 2:28 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello friends, **Only Continuous control loops Selecting an optimum sampling time of PID controllers is crucial when Processing resources of CPU is limited and several loops should be processed.There are some practical tips such as dividing processes to Slow,Medium and Fast ( Table 8.1of Controlling with SIMATIC) .But there is always degree of ambiguity in categorizing. But,there is an generally accepted rule of thumb in control literature (also mentioned in Controlling with SIMATIC) :
What do you think?Is there a way to determine the dominant time constant of a process by SIMATIC products? Best regards, Hamid Hosseini |
This contribution was helpful to1 thankful Users |
4/18/2012 4:41 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, there are some possibilities to delay the output value in refer to the input value. See the examples of the FAQ: http://support.automation.siemens.com/WW/view/de/1005801 With best regards |
This contribution was helpful to1 thankful Users |
4/18/2012 5:00 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello Cicero, This is not a question to be answered by just copying FAQ links. The link you pointed us to that is a pure delay function which is far from concept of "Time Constant". http://en.wikipedia.org/wiki/Time_constant Here, I intended to start an open discussion to find a method to estimate the dominant time constant of process .I have some possibilities in my mind but needs to be developed a bit more. Share your ideas. Best regards, Hamid Hosseini |
Follow us on