11/12/2007 2:27 PM | |
Joined: 10/31/2006 Last visit: 9/21/2022 Posts: 134 Rating: (34) |
Hi Rico, here is an exampe that I use and it works fine. Make sure you have IIS and SMTP installed on the machine you are going to send it from.
Dim S |
Last edited by: CromptonS at: 12.11.2007 14:50Last edited by: CromptonS at: 12.11.2007 14:43 |
|
3/17/2009 1:47 PM | |
Joined: 11/15/2007 Last visit: 3/23/2024 Posts: 11 Rating: (2) |
Hi, I'm trying (without any success) to run this script and send e-mails over a server which requires authentication. Anybody succeeded on this? I found these additional settings, but could not implement them: objEmail.Configuration.Fields.Item("http://schemas.microsoft.com/cdo/configuration/smtpauthenticate") =1 objEmail.Configuration.Fields.Item("http://schemas.microsoft.com/cdo/configuration/sendusername") = strUser objEmail.Configuration.Fields.Item("http://schemas.microsoft.com/cdo/configuration/sendpassword") = strPass |
Last edited by: redmaker at: 3/17/2009 1:48 PM |
|
3/17/2009 2:04 PM | |
Posts: 9 Rating: (1) |
Hi Redmaker, I send also e-mails via a mail server with username and password. Try to set the sendusing, smtpserver, smtpauthenticate items. Andcheck also the server port, which you can set with sendserverport item. Regards, Bakkertje objEmail.Configuration.Fields.Item("http://schemas.microsoft.com/cdo/configuration/sendusing") = 2 objEmail.Configuration.Fields.Item("http://schemas.microsoft.com/cdo/configuration/smtpserver") = "ServerName" objEmail.Configuration.Fields.Item("http://schemas.microsoft.com/cdo/configuration/smtpauthenticate") = 1 'SMTP server authenticatie objEmail.Configuration.Fields.Item("http://schemas.microsoft.com/cdo/configuration/sendusername") = "name" objEmail.Configuration.Fields.Item("http://schemas.microsoft.com/cdo/configuration/sendpassword") = "pwd" objEmail.Configuration.Fields.Item("http://schemas.microsoft.com/cdo/configuration/sendserverport") = 587 |
3/17/2009 3:32 PM | |
Joined: 11/15/2007 Last visit: 3/23/2024 Posts: 11 Rating: (2) |
Thank you for the immediate reply, Bakkertje. |
Last edited by: redmaker at: 3/17/2009 3:34 PM |
|
3/18/2009 11:08 PM | |
Posts: 352 Rating: (7) |
Hi, I have also been woorking some time to find a way to send sms directly from WinCC alarms. To solve this I use the send mail procedure on the sql server and a email/sms gateway. Further we set all alarms to trigger an action. Then I created a database where we store the message id's which is supposed to trigger a sms. The db also contains recievers, groups etc. When a alarm is triggered the application does a lookup in the database to find the right reciever and the send the message. To administer the system I use a small .net application The application is still under testing, but so far it works just fine. |
11/5/2009 9:18 PM | |
Posts: 33 Rating: (5) |
I know this isn't VBS but I figured I'd share, it may help. This doesn't open Outlook, rather forces the email/SMS through cmd. I call out a .BAT file if an email/SMS is needed to be sent out automatically upon tag change/alarm. Download a free program called BLAT. (follow install instructions) Then write a .BAT file like this: start /min blat -to someone@someplace.net -f alarmpanel@factory.net -server mail.someserver.net -subject "test alarm email" -body "This alarm is high, service needed, message generated from PC-0001 on Factory floor" -debug This is the route I take if only serveral alarms need to trigger an email or SMS message. You write a specific .BAT for each alarm and launch it from a hidden i/o field.(on a screen that is always active). There is a ton of ways you can push email/sms out. Also helpful is if you know the carrrier of the cell phone you are trying to SMS..See below. Alltel 10-digit phone number]@message.alltel.com Example: 1234567890@message.alltel.com AT&T (formerly Cingular) [10-digit phone number]@txt.att.net [10-digit phone number]@mms.att.net (MMS) [10-digit phone number]@cingularme.com Example: 1234567890@txt.att.net Nextel (now Sprint Nextel) [10-digit telephone number]@messaging.nextel.com Example: 1234567890@messaging.nextel.com Sprint PCS (now Sprint Nextel) [10-digit phone number]@messaging.sprintpcs.com [10-digit phone number]@pm.sprint.com (MMS) Example: 1234567890@messaging.sprintpcs.com T-Mobile [10-digit phone number]@tmomail.net Example: 1234567890@tmomail.net US Cellular [10-digit phone number]email.uscc.net (SMS) [10-digit phone number]@mms.uscc.net (MMS) Example: 1234567890@email.uscc.net Verizon [10-digit phone number]@vtext.com [10-digit phone number]@vzwpix.com (MMS) Example: 1234567890@vtext.com Virgin Mobile USA [10-digit phone number]@vmobl.com Example: 1234567890@vmobl.com Hope this helps. |
5/20/2010 12:03 PM | |
Joined: 6/9/2008 Last visit: 3/17/2021 Posts: 9 Rating: (0) |
try installing a free smtp server on the same computer where the wincc is installed. http://www.softstack.com/freesmtp.html i use it and it's very easy
|
Carlos Torres |
|
6/2/2010 11:59 AM | |
Posts: 13 Rating: (1) |
can we test this configuration on the siemens system...if yes please tell me how???? |
10/22/2010 11:00 AM | |
Posts: 2 Rating: (0) |
Hi Sonduskaisgod, thanks for sharing. May I know how do you get wincc to run the batch file?
|
Last edited by: clickndeploy at: 10/22/2010 11:15 AM |
|
5/6/2016 1:47 PM | |
Joined: 5/6/2016 Last visit: 5/22/2024 Posts: 4 Rating: (0) |
|
Last edited by: newSAILENDRA at: 5/6/2016 1:50:16 PM |
|
Follow us on