2/12/2016 12:28 PM | |
Joined: 5/23/2014 Last visit: 1/24/2023 Posts: 4 Rating: (0) |
I am trying to use the faceplate created by Siemens for Sentron Pac 3200: https://support.industry.siemens.com/cs/document/67318600/faceplates-for-the-visualization-of-sentron-pac-power-meters-for-wincc-runtime-professional?dti=0&lc=en-WW The problem is that this faceplate was made for WinCC v11. When I try to convert it to WinCC V13 SP1, it shows an error (0080:000030) = "An error occurred while upgrading the project". On log file: Uncoverted object found: name='HMI_RT_1' type='Module' (model type 'Siemens.Simatic.HwConfiguration.Hmi.Model.HmiApplicationData') parts=0xfffffffd ; bit: 0=True type 'Object' (model type 'Siemens.Automation.DomainModel.Parent4LoadableObjectsLoadInfoData'); bit: 1 =False type 'Object' (model type 'Siemens.Simatic.HwConfiguration.Model.ConfigBaseData') Is it possible that some expert from Siemens (or someone else) convert it to V13 SP1? Or that someone gives some download link with the proper version. Thank you in advance ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/12/2016 5:09:28 PMNew subject after splitting |
|
2/15/2016 12:22 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
Hello creb So on my System (TIA Portal V13 SP1 Upd7)it was possible to Migrate the Library without Errors. You can find it in Attachment. Hope it Helps Bye Murof AttachmentSentron PAC_V13_SP1.zip (479 Downloads) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to5 thankful Users |
7/9/2021 1:32 PM | |
Joined: 2/24/2020 Last visit: 3/12/2024 Posts: 3 Rating: (0) |
Just in case anyone needs it in v16.
AttachmentSentron PAC_V16.zip (160 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on