Industry Online Support
Technical Forum
3/23/2010 9:42 PM | |||
Joined: 9/27/2006 Last visit: 5/10/2024 Posts: 12257 Rating: (2666) |
Hello Taher; I hope I am answering your question correctly for your project. Step 7 has an accompanying package called S7-Graph, that allows programs to be developped in IEC 61131-3 SFC (Grafcet) language; this language was designed for sequential function programming. On the Siemens Controler portal you can have a very good introduction to the language, and links to more material: You can purchase S7-Graph either as a single add-on to Step 7,
https://mall.automation.siemens.com/FR/guest/index.asp?nodeID=5000906&lang=en
Standard Functions SFC0 (SET_CLK) and SFC1 (READ_CLK) are available in Step 7 to write/read the system clock on the S7 CPUs. Here is a FAQ that will guide you in the use of SFC1: http://support.automation.siemens.com/WW/view/en/21222026 Hope this helsp, Daniel Chartier |
||
Last edited by: dchartier at: 3/23/2010 9:43 PM |
|||
This contribution was helpful to2 thankful Users |
3/24/2010 10:45 AM | |
Posts: 34 Rating: (1) |
Dear dchartier ; Thank you for your valuable answer..so i'll go in the route of S7-graph |
Follow us on