9/15/2016 2:42 PM | |
Posts: 3 Rating: (0) |
Hi, how to set the alarm light, so that half a minute flashing (blink) a then stop flashing a start light pernamently thx for help Tom |
9/16/2016 1:27 PM | |
Posts: 3 Rating: (0) |
Hi a thx mopS04, i try use two timers to simulation blink light a then to pernamently light see attachment |
9/16/2016 1:31 PM | |
Posts: 3 Rating: (0) |
|
9/21/2016 11:35 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi tomas, isn´t this too complex for such function? you have a clock-memory marker in S7-200, too. use SM0.5 for it. This bit provides a clock pulse that is on for 0.5 seconds and then off for 0.5 seconds, for a duty cycle time of 1 second. It provides an easy-to-use delay or a 1-second clock pulse. See here the S7-200 system manual in Appendix D you have a description of all special memory bits available in S7-200. hope this helps, regards, |
FCK WAR! |
|
Follow us on