2/2/2010 4:48 PM | |
Joined: 9/23/2005 Last visit: 4/16/2021 Posts: 3911 Rating:
|
Hi, It is possible to set a time set points of a S7-1200 timer from a KTP, using a Dint variable.In PLC convert this variable from the original time scale to milliseconds unit. Before to use in the timer convert Dint to Time with T_CONV instruction.Follow there is a little example.AttachmentProject.zip (1288 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
6 thankful Users |
2/14/2012 8:40 PM | |
Posts: 10 Rating:
|
But how do you convert the milliseconds back into HH:MM:SS, so you can see the remaining time on the HMI? |
Follow us on