7/20/2020 12:48 PM | |
Joined: 4/28/2015 Last visit: 4/29/2024 Posts: 3 Rating: (0) |
Thank you for the response. Unfortunately the VIM is an older card and the EIOC is the replacement. |
7/20/2020 1:21 PM | |
Joined: 9/27/2006 Last visit: 5/12/2024 Posts: 12257 Rating: (2667) |
Hello Yusuf; Very sorry. this is just about how far I can go on this subject. If DeltaV has decided to use other means of setting up an Ethernet/IP network outside of the standard EDS files (they mention tag-based,connections) I cannot help you very much. You should contact Emerson support and ask them how you should proceed to connect a G120, either on Profinet (native) or Ethernet/IP; the following links will provide as much information on the subject as is available (on Ethernet/IP) from Siemens at this time: SINAMICS G110M, G120, G120C, G120D, G120P: EDS files for Ethernet/IP communication https://support.industry.siemens.com/cs/ww/en/view/78026217 SINAMICS G: Control of a G120 with Allen-Bradley controller (Compact/ControlLogix with RSLogix 5000) via EtherNet/IP https://support.industry.siemens.com/cs/ww/en/view/82843076 Hope thin helps, Daniel Chartier |
Last edited by: dchartier at: 07/20/2020 14:47:50 |
|
12/14/2023 8:52 AM | |
Joined: 8/21/2014 Last visit: 5/10/2024 Posts: 954 Rating: (13) |
New question published by vivek_prajapati172 is split to a separate thread with the subject How to communicate to G120. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on