9/23/2014 10:37 AM | |
Posts: 4 Rating: (0) |
Yes I checked the module order _? is different. Please give me a step by step procedure on how I can change it to the correct one. Thanks |
9/23/2014 1:39 PM | |
Posts: 4 Rating: (0) |
The module order number expected is 6ES7315-2AG10-0AB0 The module order number we are seeing says "unknown" i.e. a ???? is returned. Thanks for the assistance |
9/24/2014 11:55 AM | |
Posts: 4 Rating: (0) |
Hi ALL, Thanks for the assistance so far. Apologies a little misinformation. I checked the module order number again wrt that installed and that projected. It is the same. Module Order No. installed (the device cover) - 315-2AG10-0AB0 Module Order No. of HW config - 63S7 315-2AG10-0AB0 This CPU 315-2 DP has two other cards connected to it; the 6GK7 342-5DA02-0XE0 (ie. CP342-5 cards). Both cards also have the SF fault and Buffer fault active.On HW config when I click on the PROFIBUS DP master network (showing beside the table),I getthe???? status. Also see attached screenshot obtained via TIA toolusing our Siemens Field PG (which was connected directly to the CPU315-2 DP via MPI interface). A step by step procedure to resolving this issue, including if required the configuration steps for the Module Order No. if required will be appreciated. AttachmentSiemens issue.pdf (116 Downloads) |
Last edited by: Min_Moderator at: 9/24/2014 2:31 PMEdit name of attachment |
|
Follow us on