5/3/2017 8:17 PM | |
Posts: 4 Rating: (0) |
Hello, I know this is an old tread, but figured I write here anyway. I have been using channel 0 for over 1 year without a problem (with SFB48). Now I want to add another frequency input to channel 1. But I can't get it to count even what I try. Is there something special when not using channel 0 that I need to take into account? I use a 313C CPU so it have 3 freq input channels. I have also tested to move the frequency generator from channel 0 to channel 1 but it does not count there either. I think I have HW set up okay for channel 1, basically exact copy of HW conf for channel 0. So I'm for the time being stuck. Anybody that could give me any suggestions? Could the frequency input be broken? The input works normally if I use it as a normal digital input.
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/4/2017 4:10:30 PMNew subject after splitting |
|
7/28/2017 1:54 PM | |
Posts: 4 Rating: (0) |
Have anybody ever used any other channel than 0 for frequency measurement? I'm still not able to get it working. |
Follow us on