4/5/2016 3:30 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Do you have a screenshot of the error? |
If I could help you, you can use the RATE button. Thank you. |
|
4/5/2016 3:49 PM | |
Joined: 4/14/2006 Last visit: 4/11/2024 Posts: 75 Rating: (2) |
Here a screenshot of the message |
4/5/2016 3:58 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hmm, it looks like the SFC control is assigned to a SFC that has been deleted....But it is strange that restarting WinCC solves the issue.. What I suggest to do is compile your OS and download. Then check if the issue is solved. Maybe you can try to re-link the SFC to the SFC Control object. |
Last edited by: Oreca at: 4/5/2016 4:01:19 PMLast edited by: Oreca at: 4/5/2016 4:02:42 PMLast edited by: Oreca at: 4/5/2016 4:04:16 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on