3/23/2021 6:04 AM | |
Posts: 198 Rating: (60) |
Hello Ashadako, There are multiple ways to deal with Transition on operator request using the step control modes:
However, all the above step control modes can be changed only in MANUAL as per product design. The idea behind this is drawn from one of the thumb rules of process control in which the operator or human intervention should not be allowed when the logic (or sequence) is executing in AUTO mode. Further information can be found in the manual available for SFC in this link - SFC Manual (Refer Section 16.2.3 Hope this helps |
Last edited by: Jen_Moderator at: 03/23/2021 10:15:02Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on