Industry Online Support
Technical Forum
9/4/2012 10:41 AM | |
Posts: 139 Rating: (1) |
Hello, experts and members! As I can see here SFC84 is for CPUs with Micro Memory Card (MMC). But if I want to save DB from work memory to load memory in case of S7-400 controllers, how can I do this? Best regards, SpKV. |
9/4/2012 4:29 PM | |
Posts: 139 Rating: (1) |
Or more explicitly: can I save content of some DB (for example tunings from the OP or WinCC) from work memory to FLASH card in runtime? Best regards, SpKV. |
9/6/2012 7:32 PM | |
Posts: 947 Rating: (45) |
Hello! In CPU-4xx write on flash card in run-mode not possible. Flash card can only full overwrite |
10/13/2016 11:27 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by manhar71 is split to a separate thread with the subject How to use SFC84. Best regards |
Follow us on