10/7/2010 7:51 AM | |
Posts: 111 Rating: (0) |
Dear Yolov, I did what you had suggested. I used a free process value and set CurentUser and even CurrentUserName tags to the process valueand I made it visible in the table columns, but the only things I received were some digits that infact show my current process value, while I need to indicate current user name. I had previousely put a statistic text and attached CurrentUserName tag to it to show me the current user and it worked correctly(pic 1), but after attaching the CurentUser and CurrentUserName tagsto the processvalue, as soon as occurance of an alarm, I figured out the text doesn't show me anythingthat means it is logout.(In my project, alarm is an analog one and it has been defined upper 40.) |
10/7/2010 7:53 AM | |
Posts: 111 Rating: (0) |
Dear Yolov, I have attached the pic that shows after occuranc of alarm. thanks |
10/18/2010 1:50 PM | |
Posts: 111 Rating: (0) |
Dear BilalD, I have done it many times before, but it doesn't work. I have spent a lot of time on this case, if you are sure, please send me a project. I look forward to hearing from you. Thanks |
Follow us on