9/8/2016 10:40 PM | |
Posts: 38 Rating: (2) |
What is the value in Channel MD 20150[14], 20152[14]? The G functions screen shows the currently active G functions for each function group. It's possible that the default G code for group 15 when the channel is reset is G95 (Channel MD 20150[14]=3), which means most of the time, while the channel isn't actively running the program, it'll show G95. However, in the program, after it gets past the G94 line, the active G function page should show the updated setting of G94 as the currently active setting. Try adding an M0 after the G94 line and checking the G function screen at that point, does it show the updated G94 setting as the active G function for that group? If G95 is the default setting on channel reset, it'll revert back to G95 at the end of the program. |
Follow us on