6/5/2020 8:03 AM | |
Posts: 8 Rating: (0) |
Ok Thank you, Am getting all these information now. Will provide them shortly. |
6/5/2020 8:26 AM | |
Posts: 8 Rating: (0) |
Order No. 6ED1052-IMD00-0BA8 LSC Version 7.1 IP: 192.168.000.001 S/NetMask: 255.255.255.000 LapTop PC; IP: 192.168.020.090 SubnetMask: 255.255.255.000 |
6/5/2020 9:10 AM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32886 Rating: (4066)
|
Hello Mafak, two problems. 1.) Your LSC version is not the right for a LOGO! 0BA8. You need LSC V8.0 or higher. But if your V7.1 a full version can you upgrade for free to the actually LSC V8.2.1. The upgrade can you download here: LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) But it's 1,3 GB complete package. If you have dowload the software, start the setup as a administrator. 2.) The LOGO! and the PC are not in the same subnet. in one of the devices you must change the subnet. |
6/5/2020 9:34 AM | |
Posts: 8 Rating: (0) |
Thank you ixo65, 1.) I will now download to upgrade LSC version. 2.) I thought the subnet masks are the same. Did you mean the IP address that I need to change? |
6/5/2020 9:42 AM | |
Posts: 8 Rating: (0) |
Thanks so much for simplifying that for me to understand. Much appreciate that. |