12/23/2018 10:15 PM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2684)
|
Helo sandy; Your actual question is not clear. Are you asking if these modules will function with sensors and actuators rated 120VAC? Based on the attached extracts from the S7-300 module data, an input signal of minimum 79 VAC will be recognized as a "1" signal, so the input module will function with 110 VAC. On the output side, whatever supply you connect to the L1 connection of yhe module will be transfered when the module output is active.; if you connect 110VAC, the output will be 110 VAC when the signal is active. You can find the S7-300 module data manual in the following link and you can consult it for more ,information on the modules. : https://support.industry.siemens.com/cs/ww/en/view/8859629 If this does not answer your question, please formulate it in a clear and precise manner. Hope this helps, |
Last edited by: dchartier at: 12/24/2018 3:35:52 AMLast edited by: dchartier at: 12/24/2018 3:36:25 AM |
|
Follow us on