1/24/2017 11:03 AM | |
Joined: 3/14/2008 Last visit: 12/5/2019 Posts: 1451 Rating:
|
Hi, When using Simatic BATCH, a shared folder called: "BATCH" is created. This can be set when you install BATCH option from the DVD. I think the drive where the shared folder is referring to is full. It does not have to be the installation directory of PCS7. You can find the location by following the steps below: 1. Go to My Computer, right click and select "Manage". 2. Go to "Shared Folders"->"Shares" and see the path name for: "BATCH". This is the location of the sbsdata. Can you check if this is your problem? |
If I could help you, you can use the RATE button. Thank you. |
|
1/24/2017 11:43 AM | |
Joined: 3/14/2008 Last visit: 12/5/2019 Posts: 1451 Rating:
|
Hi Harshal7, If the available hard disk memory space of the partition on which the SIMATIC BATCH data is located drops below the value (%) of the total size of the partition, an error message is output as system message in BatchCC in addition to an error message on the PCS 7 OS. ● No new batches and no new job folders can be created. ● New batches cannot be started manually or automatically. ● No new recipes, libraries, formulas, formula categories, materials or qualities can be created. The setting should be made in BatchCC. Maybe you can find this setting and check if it is set correctly. |
Last edited by: Oreca at: 1/24/2017 11:44:03 AMLast edited by: Oreca at: 1/24/2017 11:44:32 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
2/2/2017 12:41 PM | |
Joined: 2/29/2016 Last visit: 9/18/2019 Posts: 72 Rating:
|
Thank you! I will do as you described. |
Follow us on