10/16/2018 10:00 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi Foolish_Q, did you know the application example "Configuring of SIMATIC BATCH Reports using a practical example"? This application example provides a configurable sample report template. This is based on the SIMATIC BATCH standard report. The report can be adjusted to enable report objects (headers, details, lines) to be hidden based on hierarchy levels, object types, object status, etc. Even the representation of messages can be adjusted. with regards |
10/25/2018 11:07 AM | |
Joined: 7/4/2012 Last visit: 3/19/2024 Posts: 6 Rating: (1) |
Hi Heisenberg2: Thanks . I have read the document . It seems to be a easy way. I planning to test on plant, and see if it meets the user's requirement.
|
Follow us on