1/19/2011 4:08 PM | |
Joined: 9/27/2006 Last visit: 9/25/2024 Posts: 12283 Rating: (2685)
|
Hello stefano; A quick search on Siemen's webpages has brought no new information to light, so I will have to say that the FF Link is exclusively configured with PCS 7. Mr. J_Bell is also quite definite about this: /tf/WW/en/Posts/26314 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/19/2011 4:13 PM |
|
1/19/2011 10:28 PM | |
Joined: 7/2/2008 Last visit: 9/25/2024 Posts: 928 Rating: (308)
|
Hello stefano,
Hello dchartier, I think stefano was pointing at the new SIMATIC FF Linkwhich has been just released. While MR. J_Bell was talking about the DP/FF-Linkwhich was not from SIMATIC family and is discontinued now. As you can see in its manualthe solution was specially developed for PCS7. Maybe it could be working with STEP7 but it was officially released for PCS7. However, this is different when it comes to the new SIMATIC FF Link. It'sa SIMATIC family member that's totally built & designed inside Siemens and it's built onthe specially designed IM153-2 FF. You can read in the manual that it requires either STEP7 V5.5 or PCS7 V7.1 SP2. Best regards. H-H |
This contribution was helpful to2 thankful Users |
Follow us on