6/6/2007 5:15 PM | |
Joined: 10/18/2006 Last visit: 7/29/2024 Posts: 163 Rating: (3) |
Dear Sir., We´re facing a problem related to Simatic Logon once we have installed it on our PC. We´ve already installed Simatic Logon and created the group "Logon_Administrator"; also we´ve created an user administrator and link it to this group. The first time i opened the "Simatic Logon Configure", i used the user from the local PC, but once it´s configured and it´s selected the PC where the rest of the users are created, I try to get into the "Simatic Logon Configure" and get the error message shown in the attached file (.bmp). It also happens when i try to log in WinCC with the Simatic Logon option activated. Meanwhile, if i try to search the local PC instead of the one in the network, I manage to log in. Because of this we`ve tried to change the "local security directive" from both PCs (to have access to network stations), to add the "logon_administrator" group... but it still doesn´t work. We have rebooted all PCs from every part of the process in case it´s necessary. We have reviewed and modified some of the options from the "security directive" but the error stays.
AttachmentErrorLogon.zip (502 Downloads) |
Follow us on