5/12/2009 1:18 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hello, I think we need some more information to help you out. it seems you have SIMATIC NET installed. Can you give us a version number? With that you check or your version is compatible with Windows XP SP2 or not. If it's compatible you can install it problem free if it's not compatible you could buy an upgrade which is in most cases not expensive at all. But for the correct upgrade we need the version you have at the moment. Checking this on your License Floppy is the best way... Which SIMATIC NET software component is enabled for which operating system? http://support.automation.siemens.com/WW/view/en/9859007 |
Best regards, |
|