12/1/2014 6:54 PM | |
Joined: 10/10/2014 Last visit: 2/25/2023 Posts: 8 Rating: (0) |
[Quote user="Berg"]Hello Giang, In the following links you can find informations about the comm of S7-200 and MM4 using USS protocol with example. S7200_MM4_USS_Connection MicroSet Tip 28 MicroSet Tip 65 And following a link with S7-200 and SINAMICS G110, very good doc. Micro Automation: Simple networking and cascading of drives (MAS 26) I hope this helps you !
AfrikaansAlbanianArabicArmenianAzerbaijaniBasqueBelarusianBulgarianCatalanChinese (Simplified)Chinese (Traditional)CroatianCzechDanishDetect languageDutchEnglishEstonianFilipinoFinnishFrenchGalicianGeorgianGermanGreekHaitian CreoleHebrewHindiHungarianIcelandicIndonesianIrishItalianJapaneseKoreanLatinLatvianLithuanianMacedonianMalayMalteseNorwegianPersianPolishPortugueseRomanianRussianSerbianSlovakSlovenianSpanishSwahiliSwedishThaiTurkishUkrainianUrduVietnameseWelshYiddish⇄AfrikaansAlbanianArabicArmenianAzerbaijaniBasqueBelarusianBulgarianCatalanChinese (Simplified)Chinese (Traditional)CroatianCzechDanishDutchEnglishEstonianFilipinoFinnishFrenchGalicianGeorgianGermanGreekHaitian CreoleHebrewHindiHungarianIcelandicIndonesianIrishItalianJapaneseKoreanLatinLatvianLithuanianMacedonianMalayMalteseNorwegianPersianPolishPortugueseRomanianRussianSerbianSlovakSlovenianSpanishSwahiliSwedishThaiTurkishUkrainianUrduVietnameseWelshYiddish English (auto-detected) » Hungarian AfrikaansAlbanianArabicArmenianAzerbaijaniBasqueBelarusianBulgarianCatalanChinese (Simplified)Chinese (Traditional)CroatianCzechDanishDetect languageDutchEnglishEstonianFilipinoFinnishFrenchGalicianGeorgianGermanGreekHaitian CreoleHebrewHindiHungarianIcelandicIndonesianIrishItalianJapaneseKoreanLatinLatvianLithuanianMacedonianMalayMalteseNorwegianPersianPolishPortugueseRomanianRussianSerbianSlovakSlovenianSpanishSwahiliSwedishThaiTurkishUkrainianUrduVietnameseWelshYiddish⇄AfrikaansAlbanianArabicArmenianAzerbaijaniBasqueBelarusianBulgarianCatalanChinese (Simplified)Chinese (Traditional)CroatianCzechDanishDutchEnglishEstonianFilipinoFinnishFrenchGalicianGeorgianGermanGreekHaitian CreoleHebrewHindiHungarianIcelandicIndonesianIrishItalianJapaneseKoreanLatinLatvianLithuanianMacedonianMalayMalteseNorwegianPersianPolishPortugueseRomanianRussianSerbianSlovakSlovenianSpanishSwahiliSwedishThaiTurkishUkrainianUrduVietnameseWelshYiddish
English (auto-detected) » Hungarian |
Last edited by: CS Moderator at: 12/2/2014 9:59 AMSplitting; referred post inserted Last edited by: silvius at: 12/1/2014 6:57 PM |
|
12/1/2014 11:22 PM | |
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello silvius; You can control a SinamicsG120 drive over the USS protocol. Do you have access to the USS/Modbus functions on your MicroWin libraries? Have a look at the following documents for information on USS with a Sinamics G120 drive: USS (RS485) communication between S7-200 and SINAMICS G120 SINAMICS G120 inverter with CU230P-2 Control Units(Section 7.6.2: Communication over USS protocol). Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/1/2014 11:25 PMLast edited by: dchartier at: 12/1/2014 11:25 PM |
|
This contribution was helpful to2 thankful Users |
Follow us on