11/2/2017 7:42 PM | |
Posts: 1 Rating: (0) |
Dear, good afternoon! I have a machine with a CLIP SIEMENS SIMATIC S7 300 CPU313C-2 DP. The machine was running normally and suddenly stopped and did not work again. The CLP is with the LEDs as follows: SF - On BF - blinking DC5V - On FRCE - off RUN - on STOP - off I have already done the diagnosis, attached result (Module Information) but I can not solve my problem. I have read in some posts and I have seen in some videos that it is necessary to click on "Open Block" to open the location of the error but this icon is not enabled in my diagnosis. How should I proceed? Is it possible to solve the problem by uploading the program, resetting the CLP and making a new download? Also attached are two other files I generated from the program and CPU. Please! I would very much like you to help me with this. I have the machine stopped affecting my production. Thanks! ------------------------------------------------------------------------------------------ AttachmentModule Information.pdf (241 Downloads) |
Last edited by: Jen_Moderator at: 11/3/2017 6:15:56 AMEdited text for better reading. Last edited by: Jen_Moderator at: 11/3/2017 6:18:05 AMNew subject after splitting |
|
Follow us on