6/12/2015 9:02 PM | |
Posts: 5 Rating: (0) |
silden, Hi Guys, I'm currently working on a SIMIT SF 8.1 project with a SIMBA Profibus to setup a development and station. I have only on e problem: The customer is using ASI bus for Field I/O, the problem some of the Devices are setup to run on the ASiB channel input and these don't have a specific I/O address. How should I write and read these I/O? I could write to the Instance DB of the ASiB Channel driver, but that isn't a clean solution. Thank you
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/15/2015 9:49:00 AMNew subject after splitting |
|
3/11/2016 4:05 PM | |
Posts: 63 Rating: (8) |
look at this topic https://support.industry.siemens.com/tf/us/en/posts/as-i-master-third-party/129812/?page=0&pageSize=10 |
3/11/2016 9:02 PM | |
Posts: 63 Rating: (8) |
also i could find this special table in my laptop that is from one of the german company wich i had been work with Attachmentasi -io -adress.xlsx (104 Downloads) |
Last edited by: Saeed Bahadori at: 3/11/2016 9:02:46 PM |
|
Follow us on