10/14/2021 9:03 AM | |
Joined: 3/13/2015 Last visit: 4/22/2024 Posts: 122 Rating: (38) |
Hi HajoPaj, not sure what you SIMIT version is. Here you can find the hardware requirements of V10.1: https://support.industry.siemens.com/cs/ww/en/view/109780242/135919033867 |
10/19/2021 7:31 AM | |
Joined: 1/11/2019 Last visit: 4/23/2024 Posts: 684 Rating: (139) |
Hi HajoPaj, You can check the setting in your VC machine. If the load value always jumps back and forth between two values, the problem may be that the processor of your computer keeps changing the clock frequency for energy saving reasons. You can avoid this by altering the system settings of your computer, for example. Select "Control panel > Power Options > Power plan > Advanced power settings > High performance". If the simulation load is too high, you can access information on the cause with the "SimulationLoad" component. SIMIT Simulation Platform (V10.2) Please go through the above link to know more about it & You can find additional information on the component in: SimulationLoad (Page 487) |
Follow us on