5/18/2010 8:12 PM | |
Joined: 9/27/2006 Last visit: 5/5/2024 Posts: 12257 Rating: (2666) |
Hello Mag-Ptm; You can find the Simocode Pro V GSD file in this link: http://support.automation.siemens.com/WW/view/en/113630 This will allow you to insert a Simocode Pro V DP-slave in any Profibus configurator, once you insert it. As far as the Invensys GSD file is concerned, you should look for it on the Invensys website, opr in the documentation that was provided with the system. However,I have to ask: is this Invensys system to be used as a Profibus slave as well? If it is a Profibus-DP master, you do not need a GSD file; a master device file must exist in the configurator you plan to use. hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
5/18/2010 8:21 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, Station type: SIMOCODE pro C / SIMOCODE pro V Order no.: 3UF7 000-1A*00-0 / 3UF7 010-1A*00-0 SIMOCODE_pro.ZIP About Invensys I/A GSD file refer to InFusion™ Field Device Manager for Profibus Devices (PSS 21S-10B4 B3) for additional information on IEE tools and editors for configuring, commissioning and maintaining PROFIBUS_DP networks. And now let's return to main question. What exactly do you wan to do? Give more details. Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
5/19/2010 5:50 AM | |
Joined: 10/7/2005 Last visit: 5/6/2024 Posts: 3004 Rating: (1046)
|
Hello MAG-PTM acyclic data is read out via so called Data record read request. TheyareNOT part of the cyclic "I/O" data and can NOT be found inside the GSD file NOR configured in the DP Master. You would use either SFC58/59 or SFB52/53 in an S7 PLC to read these out, but I am unfortunately unable to tell you whatblocks are availble inside your Invensys I/A system to cater for DPV1 releated acyclic data records read/writes. Please note that DPV1 releated acyclic data records read/writes is ageneral Profibus DPV1 related capability, so the first thing to check is what capabilities yourInvensys I/A systemoffers for this. Appendix B of THIS Simcode manual contains all the Data records and also some more info on this subject. I hope this helps |
Cheers |
|
5/23/2010 12:48 PM | |
Joined: 10/7/2005 Last visit: 5/6/2024 Posts: 3004 Rating: (1046) |
One would hope so dear MAG-PTM, question is if they provide youwith a mechanism to read (or write) Data Records via your user program or via a different way. As said before, Siemens proivdes pre-programmed System FC's/FB's (i.e. SFC58/59 and SFB52/53) for this purpose which you "simply" call in your user program. These System FC's/FB's are explained in THIS manual, I am somewhat doubtful though how much this Siemens relevant Blocks information will help youfor what you want to do in the Invensys system. I suggest you get in touch with Invensys andseek advise from them on how DPV1 related Data Record reads/writes are implemented/possible in their system. I hope this helps |
Cheers |
|
This contribution was helpful to2 thankful Users |