6/12/2012 12:24 PM | |
Posts: 467 Rating: (59)
|
hello Lars, question1 :please see attached screenshots question2 : the max. possible motor current, which can be set, depends on the range of the used CT. => Example : if a CT is used with measuring range 0,3 - 3A, then the max. settable motor current Ie = 3A. Please download also the manual of 3UF7 : http://support.automation.siemens.com/WW/view/de/20017780/0/en On page B-21 following you will find the data records with all possible parameters ( read / write). On page E-4 and follwing you will find typical wiring examples and its parameterization. AttachmentConfiguring Simocode.pdf (246 Downloads) |
6/12/2012 11:00 PM | |
Posts: 4 Rating: (0) |
Thanks Daniel! I think it is alittle bit odd that the result from the measurement is not in floating point :(
|
Follow us on