Industry Online Support
Technical Forum
9/1/2009 4:39 PM | |
Posts: 5 Rating: (0) |
Ok, So I have been assigned the task of providing a Client with settings for thier simocode modules that are installed within their MCC without ever having training or being able to play around with the units. Worked it out the best I could using the manuals. All the simocodes are either set up as Direct Starter, Reversing Starter, or Overload Relay. The direct and reversing starters are use for the starting of motors. The overload relay is being used in fused disconnects that feed external VFDs. Most of the settings I could figure out but I just want a sanity check on what I am providing the programmers. See attached, if someone who was to program the simocode received this would this be enough, or am I missing a critical piece of information that is required?? Do I have to worry about transfer bits/bytes?? Thanks Jeff AttachmentSimocode for Forum.pdf (557 Downloads) |
Follow us on