5/2/2016 3:05 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello With PROFINET Media Redundancy Protocol, Only one failure in the network can be handled while the machine is continuing with bumps. If Two nodes fail simultaneously the devices in between cannot communicate. Pl see the following document for more details : SIMATIC/SIMOTION/SINAMICS: PROFINET devices with media redundancy and system redundancy Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on