Industry Online Support
Technical Forum
5/24/2013 2:05 PM | |
Posts: 13 Rating: (1) |
Thank you very much for your assistance. I will reassemble the electronics, and read the the error codes asap. best regards, Nermin. |
5/25/2013 3:04 PM | |
Posts: 2964 Rating: (478)
|
Hello, Looks to be your Z axis power module is not healthy....have you checked the Diodes which are acrossed the IGBTs 300608 alarm May be coming ifthe drive output is not coming properly then only you have these fault / if the motor brake is not released / If motor is coupled with mechanics and it load too... /tf/WW/en/Posts/45570 Check this you can come to some conculsion Regards, Prakash |
This contribution was helpful to2 thankful Users |
Follow us on