9/13/2007 4:07 PM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Posts: 271 Rating:
|
Hello Daniel, Here is data regarding standard parameters for the motor you have:
Sounds like you need to recommission one of the axes. Delete the boot file and start over. Hope this helps... |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
9/17/2007 6:24 AM | |
Joined: 8/31/2007 Last visit: 10/27/2007 Posts: 14 Rating:
|
I found the problem. |
9/21/2007 5:45 PM | |
Posts: 271 Rating:
|
Hello Daniel, My recommendation is to recommission this axis. In otherwords, delete the boot file and start over. Hope this helps... |
10/17/2007 8:18 AM | |
Joined: 8/31/2007 Last visit: 10/27/2007 Posts: 14 Rating:
|
Hello! Soo I start from zero and entered all parameters. For one module I solve the problem(wrong motor code). But for the either one the problem persist. Soo i switch the control board to see if the problem is the control board or power module. But the problem persist even with the board from the similar module that works. Could be a problem from the power module or resolver? With the corect parametrization( we have one similar drive with similar motor and parameters and works fine ) and this one display on parameter 002 = 54A and we measure at drives output 35A. Thanks! |
Last edited by: daniel2007 at: 17.10.2007 08:28Last edited by: daniel2007 at: 17.10.2007 08:26 |
|