12/6/2019 11:07 PM | |
Joined: 8/4/2014 Last visit: 1/29/2024 Posts: 23 Rating: (1) |
Dear all, could some one help me with understanding attached motor nameplate? Motor is Simotics 1LE1501-3AB43-3AB4-Z, line supply is 440V/60Hz, motor connection is delta. https://mall.industry.siemens.com/mall/en/uk/Catalog/Product/1LE1501-3AB43-4AB4-Z%20L51 On motor nameplate there are two sets of nominal values for same power supply of 440V/60Hz. Which nominal parameters should be set as motor rated values in VFD? 1) 440V / 60Hz / 285A / 178kW / 0,87 / 95% / 1790rpm OR: 2) 440V / 60Hz / 255A / 160kW / 0,87 / 95% / 1790rpm Cooling medium is air with inlet temperature less than 40°C and altitude is less than 1500m. Thank you in advance!
|
Last edited by: Almen123 at: 12/07/2019 16:54:09 |
|