1/26/2014 3:47 PM | |
Joined: 3/17/2010 Last visit: 1/15/2020 Posts: 5 Rating: (0) |
Dear All, Hope you’re ok, I need to use the absolute encoder “retained value” and “correction” properties only (just take advantage of encoder natural benefits), to make PLC DIRECT CONTROL over the drive. Function Manual FH1 talks about activate POSITION CONTROLLER to have access granted to encoder calibration parameters and also to have access to its correction module. Actually I’m using SPEED CONTROL MODE between this drive(sinamics S120 Single momo)and a S7-300 controller (315-2PN/DP), I have elaborated following procedure with objective to obtain your expert help for validation, because Equipments are so far from me and don’t have form to put this in practice, may be If you have done this could tell me if I’m on the right way or if another things are necessary or if I'm wrong and it's not the mode, Document was done with Simotion SCOUT. please help me how to make this possible... Think this case could contribute considerably to community. Thanks for all your time and collaboration. AttachmentELLABORATED PROCEDURE.pdf (109 Downloads) |
Last edited by: Ing. Ronnie at: 1/26/2014 3:53 PM |
|
Follow us on