5/9/2008 5:12 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, yes the FB works for all Linemodules which supports telegram 370. Regards Christoph |
9/1/2008 1:52 PM | |
Joined: 8/6/2008 Last visit: 10/8/2008 Posts: 12 Rating: (1) |
Hello, I needed to use 200 kwt BLM when they just were issued. That times I did not find any FBs and made an easy programby myself (see att.) Used 370 telegram: Input word (from BLM):infeed_status Огезге word (ещBLM):infeed_control The infeed in ready for operation IF((infeed_status = 16#1a97 )OR (infeed_status = 16#1a17 )) Pretty simple - works 2,5 years. Regards! AttachmentInfeed control in xml.zip (584 Downloads) |