1/10/2017 12:10 AM | |
Posts: 305 Rating: (2) |
does simotion can via drive-cliq connect smc encoder working master encoder ? is config smc axis must config driver first ? |
1/10/2017 1:33 AM | |
Posts: 1529 Rating: (202) |
1. Yes 2. Yes, configure the External Encoder in Sinamics Integrated first before External Encoder in SIMOTION |
1/10/2017 4:32 AM | |
Posts: 1529 Rating: (202) |
You need to create your Sinamics Integrated controller first. |
1/10/2017 4:42 AM | |
Posts: 305 Rating: (2) |
in test ,wo has not S120, can i to use SIMOTION D425 connect SMC ? |
1/10/2017 5:37 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
YES |
1/10/2017 6:08 AM | |
Posts: 1529 Rating: (202) |
Yes, should work fine. |
1/10/2017 6:37 AM | |
Posts: 1529 Rating: (202) |
Looks OK. No need to create a drive or an infeed. Just Encoder. Then you can attach the TO External Encoder from SIMOTION. |
Follow us on