5/30/2018 3:39 PM | |
Joined: 3/2/2007 Last visit: 4/12/2024 Posts: 924 Rating: (5) |
Does the S110 control unit CU305 work with power modules PM250 also ? 6SL3225-0BE33-7AA0 , SINAMICS G120 POWER MODULE PM250 WITH BUILT IN CL. A FILTER POSSIBILITY OF REGENERATION 3AC380-480V +10/-10% 47-63HZ OUTPUT HIGH OVERLOAD: 37KW FOR 200% 3S,150% 57S,100% 240S AMBIENT TEMP 0 TO +50 DEG C OUTPUT LIGHT OVERLOAD: 45KW FOR 150% 3S,110% 57S,100% 240S AMBIENT TEMP 0 TO +40 DEG C 635 X 275 X 204 (HXWXD), FSE PROTECTION IP20 WITHOUT CONTROL UNIT AND BOP |
Last edited by: Ziemens at: 5/30/2018 3:40:49 PM... thank you ... |
|
5/30/2018 3:53 PM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22213 Rating: (2979)
|
Hello, no this combination is not possible. |
Follow us on