7/10/2018 2:46 PM | |
Joined: 10/11/2006 Last visit: 4/24/2024 Posts: 5823 Rating: (789)
|
Hello, With the PROFINET functionality I-Device, up to 1440 bytes of user data can be transferred in each direction between the IO controller and I-Device. The user data is made up of input or output data + user data supplement. A submodule of the SIMOTION I-Device can have a maximum size of 254 bytes. 3.1.4 I-Device https://support.industry.siemens.com/cs/ww/en/view/38494882 |
With best regards, |
|
Follow us on