11/19/2021 3:11 PM | |
Joined: 5/7/2008 Last visit: 7/10/2024 Posts: 30 Rating: (1) |
|
11/20/2021 7:13 AM | |
Joined: 5/7/2008 Last visit: 7/10/2024 Posts: 30 Rating: (1) |
because the x127 port does not support i-device communication. Our first priority is to communicate over the x127 port. |
11/23/2021 5:52 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
PU/GET not supported from Simotion you can use Open user Communication with TCPSend and TCPReceive. |
11/23/2021 9:25 AM | |
Joined: 10/18/2016 Last visit: 8/28/2024 Posts: 21 Rating: (1) |
As ChristophD already wrote, PUT/GET is not supported with Simotion. I'd recommend to use either LCom or OPC UA. (SIMOTION Server and SIMATIC Client). |
12/1/2021 12:46 PM | |
Joined: 5/7/2008 Last visit: 7/10/2024 Posts: 30 Rating: (1) |
hello, thank you for your reply. Do you have a sample project related to tcp connection? Do we need to make any settings on the s71500 side? How do we define the s71500 addresses on the Simotion side? I will prepare and upload a program in tiaportal v15.1 for you to process.
Attachmentsimotion.zip (545 Downloads) |
Follow us on