2/7/2012 11:43 AM | |
Posts: 6 Rating:
|
Dear Friends,
In our machine having Incremental Encoder for Position, the Same Incremental Encoder connected at Simotion D410-X23 Connector.
This is a linear application.
1PH7 motor-- --- connected to - Gear Box (11Rev of motor = 1 Rev. of Gearbox Output) – connected-------- with Linear movements Tables (On the Table, we are having Incremental Encoder for Position measuring, Encoder ; 2500 PPR, TTL)
Our Encoder circumference: 250mm
Motor Gear Box Ratio: 11:1
If Gear Box rotates one revolution then Table moves 610mm.
……………………………………………………………………………………………………………………………………………………………………………………………………….
We are checking with control panel, While checking – we are facing the below problems,
Attachmentdevon_tt.zip (126 Downloads) |
Follow us on