2/11/2013 2:07 PM | |
Posts: 7 Rating: (1) |
Hello, it is alsopossible to share the I/Os of an ET200S CPU with SIMOTION CPUs! The ET200S CPU has to be an I-Device for a higher-level controller, which should get access to the I/Os. In the I-Device configuration you can choose the I/Os that should be also accessible by the higher-level controller (for example SIMOTION CPU). Pleasenote that one input canbe read byboth controllers at the same time, butthe outputs canonly be written by one controller! This functionality is called "Translucend periphery" that is only existing for the ET200S and ET200pro CPU. See also following link: http://support.automation.siemens.com/WW/view/en/47247158 Best regards, I DT MC Profinet Team |
Last edited by: I DT MC Profinet Team at: 2/11/2013 2:10 PM |
|
This contribution was helpful to1 thankful Users |