Industry Online Support
Technical Forum
11/29/2013 1:09 PM | |
Posts: 76 Rating: (0) |
hello dear I'm having problems with d425 and sinamics simotion. pull for in a configuration to start testing a servo and sinamics stay offline and cpu to stop happened. went back to reload the previous configuration, but I still offline sinamics, that's because the cpu was stop? maybe it's for some config in NetPro, I will use communication speed of 6Mb dp2/mpi in NetPro, maybe that's why the cpu hangs. I think I'm going to restore everything to factory settings and start loading the config a bit, I could not even make the commissioning of the servo .... as I do a factory reset from the front panel program ... and photo attached config to see if there are any suggestions, I am concerned this from sinamics integrated offline
Attachmentsinamics offline.zip (187 Downloads) |
5/20/2014 6:19 PM | |
Posts: 76 Rating: (0) |
mr. tell me do you have any manual (handbook) or information for i can developed this commissioning. for example step by step. thanks
|
Follow us on