1/12/2017 5:34 AM | |
Joined: 7/1/2015 Last visit: 1/2/2024 Posts: 15 Rating: (0) |
Hi Christoph, I was Checking the program in online mode, suddenly the hole of green color coupling in scout project went to red color state then i clicked offline button and online button again then i faced to this big problem that when i click online button it goes to online but immediatly comes back to offline and reports the strange target system output.I can reach online mode in HW Cofig and i can read data in opc scout also the HMI and process are working perfect.i tested the other X127 and X130 but the result was the same. you can see the target system output in attach. AttachmentTarget system output.txt (69 Downloads) |
1/12/2017 8:10 AM | |
Joined: 7/1/2015 Last visit: 1/2/2024 Posts: 15 Rating: (0) |
At first should i sure after switch off and on the device will go to running state or not.because now every thing working, only i can not go online. I can go online with HW config of this project.I send diagnostic massage from D425 in attach. AttachmentDiagnose.txt (60 Downloads) |
1/12/2017 8:22 AM | |
Joined: 7/1/2015 Last visit: 1/2/2024 Posts: 15 Rating: (0) |
is it possible somebody locks the device as you told me in previous post?if yes how can i know or find it out. |
Follow us on