12/30/2016 9:16 AM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
Hello, SIEMENS just make the release for SCOUT 4.5 (do you think, they would do a new version if it should retired)? https://support.industry.siemens.com/cs/ww/de/view/109742328 There some features like object orientated programming (OOP). Also a book is written for that: https://support.industry.siemens.com/cs/ww/de/view/109742819 For high end Motion Control applications SIMOTION is the best (and for machine tool´s a SINUMERIK). But I think there are a lot of customers which prefer SIMATIC, so they can use it, if the motion control functionality is sufficient. You see the same on the drive´s. First the SINAMICS S120 was for motion control and G120 for pump´s and fan´s. Now a middle range drive V90 is on the market and a G120 with CU250S can handle positioning applications. So there is a smooth transition over the systems. Best regards Zako . |
This contribution was helpful to1 thankful Users |
Follow us on