3/19/2013 11:09 PM | |
Joined: 6/4/2008 Last visit: 9/15/2024 Posts: 1497 Rating: (324) |
Hey Christoph, please see the file I have been working on. I have given a Skydrive Link as the file is > 5MB, see linkHERE It uses the latest DCM's and a D435-2 using Scout 4.3. I tested the axis commands in an MCC program and I think I can connect to the DCM's. Is this what you mean? Regards, Graeme
|
10/26/2015 9:42 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Mori212 is split to a separate thread with the subject Replace the control of a flying saw cutter machine. Best regards |
Follow us on